earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: CRS-HH-REL-10, RP-C, RP-C-EXT-0-10V-4, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-BL-SMI-2-LV-PD, RP-C-EXT-BL-SMI-4-HV-PD, RP-C-EXT-DALI, RP-C-EXT-DALI-M-PD, RP-C-EXT-IS-BLE, RP-C-EXT-MS-BLE, RP-C-EXT-REL-4
功能: 硬件
产品版本: 2022, 2023, 2024, 7.0
2022/4/5

RP Controller Expansion Module Maintenance Modes

The RP controller expansion modules support different modes that can be used for maintenance purposes.

The following maintenance modes are supported:

  • Offline maintenance mode

  • Online maintenance mode

The Status LED on the RP controller expansion modules indicates when the device is in maintenance mode, provided that the LED is configured in show status mode (default mode). 有关更多信息,请参阅 RP Controller Expansion Module LEDs .有关更多信息,请参阅 RP Controller Expansion Sensor Module LED .

Offline maintenance mode

The device enters maintenance mode and goes offline when you configure the room bus address 0 for the device using its rotary switch.

Online maintenance mode

In online maintenance mode, the device will be online but without running any software other than what makes it possible to read diagnostics from the device and to upgrade the device.

有关更多信息,请参阅 Configuring an RP Controller Expansion Module into Online Maintenance Mode .

  • RP Controller Expansion Modules
  • Light Modules
  • Blind Modules
  • Relay Modules
  • Sensor Modules
  • RP-C-EXT-DALI-M-PD
  • RP-C-EXT-0-10V-4-PD
  • RP-C-EXT-BL-4-HV-PD
  • RP-C-EXT-BL-2-LV-PD
  • RP-C-EXT-DALI
  • RP-C-EXT-0-10V-4
  • RP-C-EXT-BL-SMI-4-HV-PD
  • RP-C-EXT-BL-SMI-2-LV-PD
  • RP-C-EXT-REL-4
  • CRS-HH-REL-10
  • RP-C-EXT-MS-BLE
  • RP-C-EXT-IS-BLE
  • RP Controller Expansion Module LEDs
  • RP Controller Expansion Sensor Module LED
  • Configuring an RP Controller Expansion Module into Online Maintenance Mode
  • RP-C Room Bus
  • Connecting RP Controller Expansion Modules to an RP Controller
  • RP Controller Expansion Module Room Bus Addressing
  • Configuring the Room Bus Address for an RP Controller Expansion Module
  • Configuring the Room Bus Address for an RP Controller Expansion Sensor Module
  • RP Controller Expansion Module Diagnostics
  • Retrieving RP Controller Expansion Module Diagnostics