WebStation is your web-based interface to your EcoStruxure BMS. You use WebStation to perform work on a daily basis in the EcoStruxure BMS.
WebStation has a many functions that help you work efficiently. You can search for and organize objects, and you can get help using the online help.
Pour plus d'informations, voir Fonctions de base .
You are notified by alarms when some important event occurs. For example, if the temperature is too low or too high in a building, if a window is open, or if something is broken, such as a fan. The system administrator sets up the alarms and decides to whom the alarm is sent.
Pour plus d'informations, voir Mode de fonctionnement des alarmes .
You can drag objects to the Watch pane to monitor their live values.
Pour plus d'informations, voir Volet d'affichage dans WebStation .
All system events, as well as information and circumstances, are recorded in the Event log. These event records can be viewed in the Events pane or in an Event View.
Pour plus d'informations, voir Mode de fonctionnement des événements .
You use trend logs to record values from devices, such as sensors. A trend log can also log consumptions, such as energy consumption or water consumption.
Pour plus d'informations, voir Mode de fonctionnement des journaux de tendance .
Schedules are used to schedule the operation of parts of the BMS, such as a device or a setpoint. For example, a you can set up a schedule to make a device to operate between 08:00 and 17:00 every workday.
Pour plus d'informations, voir Comment fonctionnent les programmes horaires .
You use graphics to display building overviews, display the status of detectors and alarms, display the value of sensors, or change setpoints. A graphic can also contain links to trend charts, trend log lists, Internet sites, or views in WorkStation and WebStation.
Pour plus d'informations, voir Mode de fonctionnement des graphiques .
You can open documents stored on an EcoStruxure BMS server using the default program associated with the file type. For example, a txt-file opens Notepad and a ppt-file opens PowerPoint.
Pour plus d'informations, voir Mode de fonctionnement des documents .
Dashboards are a way to get a graphical overview of values and logs in your system.
Pour plus d'informations, voir Fonctionnement des tableaux de bord .
You can create backups of the server using WebStation. The backup can be downloaded from the server.
There are a number of differences in functionality between WebStation and WorkStation.
Pour plus d'informations, voir WebStation and WorkStation Differences .