The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to MP and RP controllers. You plug the SpaceLogic Bluetooth Adapter into the corresponding SpaceLogic Sensor to connect to the controller. The adapter communicates with the BACnet/IP controller over the sensor bus using an RS-485 cable.
For more information, see Connecting SpaceLogic Sensor Devices to an MP Controller
.
Notice
|
SPACELOGIC SENSOR OR OTHER EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
For more information, see Commission Mobile Application Overview
.
action_zoom_plus_stroke
Figure:
SpaceLogic Bluetooth Adapter connectivity
RP Controller Onboard BLE
You can use Bluetooth Low Energy (BLE) to connect both RP and MP controllers. BLE provides you with the ability to commission BACnet/IP controllers before there is an IP network infrastructure configured and also improves on-site commissioning times and productivity. With the RP controller, you connect using its onboard BLE or the BLE adapter and the SpaceLogic Sensor. In the MP controller, you connect using the Commission mobile application BLE adapter through the controller's sensor bus.
For more information, see RP Controller Onboard BLE
.
Connecting to a Controller with the SpaceLogic Bluetooth Adapter
The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to SpaceLogic and Easylogic Controller models. To connect to a device through the SpaceLogic Bluetooth Adapter, you must wire a SpaceLogic Sensor to the controller.
For more information, see Connecting to a Controller with the SpaceLogic Bluetooth Adapter
.
Changing the PIN of the SpaceLogic Bluetooth Adapter
You change the PIN of the SpaceLogic Bluetooth Adapter for best security practices. The SpaceLogic Bluetooth Adapter PIN is engineered to a default code of 333666 and should be changed to a secure code before you perform device commissioning.
For more information, see Changing the PIN of the SpaceLogic Bluetooth Adapter
.
SpaceLogic Bluetooth Adapter LED Functionality
The SpaceLogic Bluetooth Adapter LED light displays different sequences to indicate the various functionality.
For more information, see Bluetooth LED Functionality
.