152 Topic(s)
Day mode is intended to be changed a few times a day. When day mode has been enabled or disabled, you cannot immediately toggle it again.
In the address table, double-click the cell in the Output function or Output function 2 column to see a menu of available output functions.
It is common practice to reduce the risk of false alarms by disabling detectors, or decreasing their sensitivity, in building areas where the normal activities create phenomena that resemble fires.
Faults and maintenance alerts comprise a text and a code. They are displayed on the panel, in EcoStruxure Fire Expert, and in EcoStruxure Fire Operation.
In a fire detection system, there are different types of alarms, faults, maintenance alerts, tests, and disablements. Various causes generate these alarms and changes in device states.
Use the Checking Entitlement dialog box check the content on the entitlement.
You add the entitlement to view the License Products available for activation on field servers.
Different types of alarms and maintenance alerts in a fire detection system are generated either manually or by devices, as they react to changes in their surroundings. The alarms and maintenance alerts belong to different system alarm categories.
Fire detection system objects such as fire detection panels, loop devices, and zones, are configured and interact with each other to provide the necessary features to the fire detection system.