You can use a wireless access point to connect the eCommission SmartX Controllers mobile application to the SmartX IP controller network.
Confirm that the access point is connected to a wired network containing a DHCP server.
Configure the network settings on the mobile device running the eCommission application to connect to the WiFi network containing the SmartX IP controllers.
On the mobile device, enable WiFi and then connect to the wireless network.
In the eCommission application, on the Select Connection view, tap the WiFi icon
In the Device List view, select the SmartX IP controllers to make the connection.
The Device List view allows you to easily find and select the appropriate controllers:
You can filter the device list by controller model. If you are logged in as a Flow Balancer, the device list is automatically filtered to show only MP-V controllers.
When using functions that can be applied to multiple controllers at once, you can use multi-select to choose two or more controllers.
Using the eCommission application, you can now perform tasks on the connected SmartX IP controllers as needed.