earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : WebStation
Fonctionnalités : Fonctionnalité de base
Version produit : 2023
16/02/2023

Dashboard Widgets

arrow1_rotationClone Widgets and Rebind Widget References arrow1_rotationEmpty Space arrow1_rotationAlarm Count arrow1_rotationAlarm Pareto Chart arrow1_rotationAlarm Pie arrow1_rotationAlarm Sankey Chart arrow1_rotationEvent Pareto Chart arrow1_rotationEvent Pie arrow1_rotationEvent Rate Chart arrow1_rotationEvent Sankey Chart arrow1_rotationHeat Map arrow1_rotationLog Gauge arrow1_rotationLog Pie arrow1_rotationLog Value arrow1_rotationPeriod Chart arrow1_rotationPeriod over Period Chart arrow1_rotationPoint Gauge arrow1_rotationPoint Pie arrow1_rotationPoint Value arrow1_rotationXY Plot arrow1_rotationBrowse arrow1_rotationDynamic Dashboad Widget arrow1_rotationGraphics arrow1_rotationHyperlinks

Dashboard widgets are small applications in a dashboard. Dashboard widgets are the main components in a dashboard and present graphical information from your system.

You can create one or many dashboard widgets in a dashboard. Dashboard widgets can only be created in a dashboard in WebStation.

Ready to use

All dashboard widgets are ready to use. The only thing you must do is add the trend log, variable, alarm, or event you want to display in the dashboard widget. All dashboard widgets have default setting for color and different layout components, but you can also configure them to suit your needs. For example, you can add captions to the widget itself or the x- and y-axis in diagram, you can use different colors for different values or value ranges in a gauge.

Clone Widgets and Rebind Widget References

You can clone widgets and rebind widgets references.

Pour plus d'informations, voir Cloner des widgets et relier les références des widgets .

Empty Space

Empty space is not a dashboard widget but a way to create empty spaces between dashboard widgets. Empty spaces are used when you do the layout of a dashboard.

Alarm Count

An alarm count displays the number of alarms from the EcoStruxure Building Operation system.

Pour plus d'informations, voir Nombre d'alarmes .

Alarm Pareto Chart

An alarm Pareto chart is a graphical representation of alarms represented by bars but also by a cumulative line. An alarm pareto chart gives you a quick overview of the most common causes of alarms.

Pour plus d'informations, voir Diagramme Pareto alarme .

Alarm Pie

An alarm pie chart is a circular graphic divided into slices to illustrate proportions of alarms.

Pour plus d'informations, voir Graphique circulaire d'alarmes .

Alarm Sankey Chart

An alarm Sankey chart is used to graphically present a Sankey chart of the alarms in the EcoStruxure Building Operation system.

Pour plus d'informations, voir Graphique Sankey alarme .

Event Pareto Chart

An event Pareto chart is a graphical representation where the events are represented by bars but also by a cumulative line. An event pareto chart gives you a quick overview of the most common events.

Pour plus d'informations, voir Graphique Pareto événement .

Event Pie

An event pie chart is a circular graphic divided into slices to illustrate proportions of events.

Pour plus d'informations, voir Event Pie .

Event Rate Chart

An event rate chart is a graphical representation of event rates represented by bars.

Pour plus d'informations, voir Graphique taux d'événements .

Event Sankey Chart

An events Sankey chart is used to graphically present a Sankey chart of the events in the EcoStruxure Building Operation system.

Pour plus d'informations, voir Graphique Sankey événement .

Heat Map

A heat map is a graphical representation of data where the values contained in a matrix are represented as colors.

Pour plus d'informations, voir Carte thermique .

Log Gauge

A log gauge displays trend log values in a gauge.

Pour plus d'informations, voir Jauge d'enregistrement .

Log Pie

A log pie chart is a circular graphic divided into slices to illustrate proportions of trend logs.

Pour plus d'informations, voir Graphique circulaire d'enregistrement .

Log Value

A log value displays one or many trend log values as numerical values.

Pour plus d'informations, voir Valeur d'enregistrement .

Period Chart

A period chart is used to compare trend logs over different time periods.

Pour plus d'informations, voir Graphique de période .

Period over Period Chart

A period chart is used to compare trend logs over different time periods.

Pour plus d'informations, voir Graphique période sur période .

Point Gauge

A point gauge is used to graphically display a current value in a gauge.

Pour plus d'informations, voir Jauge de point .

Point Pie

A point pie chart is a circular graphic divided into slices to illustrate proportion of values.

Pour plus d'informations, voir Graphique circulaire de point .

Point Value

A point value is used to display the present value of one or many variables as a numerical value.

Pour plus d'informations, voir Valeur de point .

XY Plot

A XY plot, also called a scatter plot, is used to display values for two trend logs.

Pour plus d'informations, voir Plan XY .

Browse

Use Browse to navigate to a graphic or a hyperlink that you want to add to a dashboard.

Dynamic Dashboad Widget

Dynamic widgets is a way to automatically add graphics to a dashboard using a search function.

Pour plus d'informations, voir Widgets dynamiques .

Graphics

Graphics can be added to a dashboard.

Pour plus d'informations, voir Graphiques sur les tableaux de bord .

Hyperlinks

Hyperlinks can also be added to a dashboard. To be able to display the content of the hyperlink, you must enable external content to be embedded in WebStation.

Pour plus d'informations, voir Configuring Security in WebStation using WorkStation .

  • Fonctionnement des tableaux de bord
  • Cloner des widgets et relier les références des widgets
  • Clonage d'un widget de tableau de bord
  • Relier les références des widgets
  • Nombre d'alarmes
  • Diagramme Pareto alarme
  • Graphique circulaire d'alarmes
  • Carte thermique
  • Jauge d'enregistrement
  • Graphique circulaire d'enregistrement
  • Valeur d'enregistrement
  • Graphique de période
  • Graphique période sur période
  • Jauge de point
  • Graphique circulaire de point
  • Valeur de point
  • Plan XY
  • Widgets dynamiques