earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : WebStation
Fonctionnalités : Dashboards
Version produit : 2022, 2023
14/03/2024

Clonage d'un widget de tableau de bord

Vous pouvez cloner des widgets déjà existants.

Afficher plus
action_close

Dashboard widgets are small applications in a dashboard. Dashboard widgets are the main components in a dashboard and present graphical information from your system.

You can create one or many dashboard widgets in a dashboard. Dashboard widgets can only be created in a dashboard in WebStation.

Ready to use

All dashboard widgets are ready to use. The only thing you must do is add the trend log, variable, alarm, or event you want to display in the dashboard widget. All dashboard widgets have default setting for color and different layout components, but you can also configure them to suit your needs. For example, you can add captions to the widget itself or the x- and y-axis in diagram, you can use different colors for different values or value ranges in a gauge.

Clone Widgets and Rebind Widget References

You can clone widgets and rebind widgets references.

Pour plus d'informations, voir Cloner des widgets et relier les références des widgets .

Empty Space

Empty space is not a dashboard widget but a way to create empty spaces between dashboard widgets. Empty spaces are used when you do the layout of a dashboard.

Alarm Count

An alarm count displays the number of alarms from the EcoStruxure Building Operation system.

Pour plus d'informations, voir Nombre d'alarmes .

Alarm Pareto Chart

An alarm Pareto chart is a graphical representation of alarms represented by bars but also by a cumulative line. An alarm pareto chart gives you a quick overview of the most common causes of alarms.

Pour plus d'informations, voir Diagramme Pareto alarme .

Alarm Pie

An alarm pie chart is a circular graphic divided into slices to illustrate proportions of alarms.

Pour plus d'informations, voir Graphique circulaire d'alarmes .

Alarm Sankey Chart

An alarm Sankey chart is used to graphically present a Sankey chart of the alarms in the EcoStruxure Building Operation system.

Pour plus d'informations, voir Graphique Sankey alarme .

Event Pareto Chart

An event Pareto chart is a graphical representation where the events are represented by bars but also by a cumulative line. An event pareto chart gives you a quick overview of the most common events.

Pour plus d'informations, voir Graphique Pareto événement .

Event Pie

An event pie chart is a circular graphic divided into slices to illustrate proportions of events.

Pour plus d'informations, voir Event Pie .

Event Rate Chart

An event rate chart is a graphical representation of event rates represented by bars.

Pour plus d'informations, voir Graphique taux d'événements .

Event Sankey Chart

An events Sankey chart is used to graphically present a Sankey chart of the events in the EcoStruxure Building Operation system.

Pour plus d'informations, voir Graphique Sankey événement .

Heat Map

A heat map is a graphical representation of data where the values contained in a matrix are represented as colors.

Pour plus d'informations, voir Carte thermique .

Log Gauge

A log gauge displays trend log values in a gauge.

Pour plus d'informations, voir Jauge d'enregistrement .

Log Pie

A log pie chart is a circular graphic divided into slices to illustrate proportions of trend logs.

Pour plus d'informations, voir Graphique circulaire d'enregistrement .

Log Value

A log value displays one or many trend log values as numerical values.

Pour plus d'informations, voir Valeur d'enregistrement .

Period Chart

A period chart is used to compare trend logs over different time periods.

Pour plus d'informations, voir Graphique de période .

Period over Period Chart

A period chart is used to compare trend logs over different time periods.

Pour plus d'informations, voir Graphique période sur période .

Point Gauge

A point gauge is used to graphically display a current value in a gauge.

Pour plus d'informations, voir Jauge de point .

Point Pie

A point pie chart is a circular graphic divided into slices to illustrate proportion of values.

Pour plus d'informations, voir Graphique circulaire de point .

Point Value

A point value is used to display the present value of one or many variables as a numerical value.

Pour plus d'informations, voir Valeur de point .

XY Plot

A XY plot, also called a scatter plot, is used to display values for two trend logs.

Pour plus d'informations, voir Plan XY .

Browse

Use Browse to navigate to a graphic or a hyperlink that you want to add to a dashboard.

Dynamic Dashboad Widget

Dynamic widgets is a way to automatically add graphics to a dashboard using a search function.

Pour plus d'informations, voir Widgets dynamiques .

Graphics

Graphics can be added to a dashboard.

Pour plus d'informations, voir Graphiques sur les tableaux de bord .

Hyperlinks

Hyperlinks can also be added to a dashboard. To be able to display the content of the hyperlink, you must enable external content to be embedded in WebStation.

Pour plus d'informations, voir Configuring Security in WebStation using WorkStation .

Pour cloner un widget de tableau de bord
  1. Cliquez avec le bouton droit sur le tableau de bord, puis cliquez sur Modifier le tableau de bord .

  2. Dans la barre d'outils Tableau de bord , cliquez sur le bouton Sélectionner des articles

     
    action_zoom_plus_stroke
    .

  3. Sélectionnez le widget que vous souhaitez cloner en cochant la case dans le widget.

  4. Cliquez sur le bouton Cloner les articles sélectionnés

     
    action_zoom_plus_stroke
    .

  • Fonctionnement des tableaux de bord
  • Dashboard Widgets
  • Barre d'outils Tableau de bord
  • Boîte de dialogue Widget – Onglet Agencement
  • Ajout d'un widget à un tableau de bord